DLPU114A August 2024 – November 2024 DLPC8445
Set Blendmap Offset Values | |
---|---|
Write Parameter(s) | |
Byte | Description |
Byte 0 |
Color Channel Select 0 = Green color 1 = Red color 2 = Blue color |
Bytes 1-2 |
Start index in the table for the data to be written |
Bytes 3 - * |
Offset of control points.The format of input should be such that the offset values are in the internal floating point format of s1m7e4. |