DLPU114A August 2024 – November 2024 DLPC8445
This command returns the current video source and the status of the source being displayed.
The command indicates whether the system is displaying an internal source, if it is trying to detect an external source, if it has detected an external source, or if it is in standby mode. This command can be used by the host processor to query the status at any point in time and take the necessary action. It is expected that the host will use this command after setting up the required source and ensure that the source validity is established before setting it up for display or reading the detected timings.