DLPU115B january 2022 – march 2023 DLPC3421
Table 3-61 describes the return parameters.
Parameter Bytes | Description |
---|---|
Byte 1 | Red LED current parameter (LSByte) |
Byte 2 | Red LED current parameter (MSByte) |
Byte 3 | Green LED current parameter (LSByte) |
Byte 4 | Green LED current parameter (MSByte) |
Byte 5 | Blue LED current parameter (LSByte) |
Byte 6 | Blue LED current parameter (MSByte) |
The parameters returned by this command have a resolution of 10 bits, and are defined by the appropriate DLPA200x specification.
When the CAIC algorithm is enabled using the LED Output Control Method command:
Use of this command is only appropriate when the LED output control method is set to CAIC (automatic) RGB LED current control.
Unused most significant bits are set to 0.