DLPU115B january 2022 – march 2023 DLPC3421
Table 3-132 describes the return parameters.
Parameter Bytes | Description |
---|---|
Byte 1 | Data byte 1 |
Byte 2 | Data byte 2 |
Byte 3 | Data byte 3 |
Byte 4 | Data byte 4 |
Byte 5 … n | Data byte 5 … n |
The flash data length command must be used to specify how much data is to be read by the read flash continue command.
The read flash start command is used to read up to 256 bytes of data starting at the specified address, or at the first address of the data type selected. If more than 256 bytes are to be read, the read flash continue command must be used. Up to 256 bytes of data can be read with each read flash continue command, which starts at the end of the last data read.
While flash processing requires that flash commands be executed in the proper order (for example, flash must be erased prior to being written), due to the flexibility provided for flash updates, command order checking is not provided.