DLPU125 june 2023
The Excel spreadsheet dlpc910_apps_fpga_luts_coe.xlsx was used to create the look up tables for DLP9000X, DLP9000XUV, and DLP6500 DMDs. The look-up tables are addressed by the DMD row that is being loaded. For each DMD row, the LUTs indicate if the row address is for last row in a mirror block. The last row indicator is used by the loader state machine to request an MCP reset for the block that just completed loading. NS FLIP, phased reset mode (x1, x2, x4), and load4z are all accommodated by the table. The block address is also included in the table for forwarding to the DLPC910.
The excel file contains four worksheets, two for DLP9000X - DLP9000XUV DMDs and two for DLP6500 DMDs. For each DMD, the first worksheet creates the LUT data per row address. The second worksheet simply copies the LUT data for export to a CSV file. Then add the .coe header and footer information using a text editor.