DLPU131A November 2023 – September 2024
The DLPC3421 Display Controller flash memory is pre-programmed with a control program binary file.
The EVM GUI can be used to generate a new binary file for programming based on selected options provided in the GUI. The new binary file can be programmed using the GUI over the UART interface.
Refer to the following documentation links for more detailed information: