Download and install the
TI UniFlash flash programming tool (version 8.4.0 or later) from TI.com
at https://www.ti.com/tool/UNIFLASH.
Launch the
UniFlash.exe
Note:
The XDS110
firmware must be updated to v3.0.0.26 (or newer) to support the
MSPM0 devices. The XDS firmware can be updated using the
UNIFLASH programming tool.
In the New Configuration
tab, select the MSPM0G3507 device, and Texas Instruments
XDS110 USB Debug Probe connection:
Click the Start
button.
Browse for and select the
DLPDLCR160CPEVM_RevE19.out (or later) image.
Click the Load
image button, and wait for the Load Program routine to
complete.
Once the Load is completed successfully, click the Verify Image
button.
If the verification is
reported successful in the Console, then the flash programming of the
MSPM0 is complete. If verification fails, then recheck setup and
connections and retry programming.