DLPU137 April 2024
The DLP4620SQ1EVM kit contains the cables and Cheetah USB to SPI adapter listed in Table 3-10 and shown in Figure 3-5.
NAME | REFERENCE | QUANTITY |
---|---|---|
Photodiode cable |
A | 1 |
Input power cable | B | 1 |
Host SPI cable | C | 1 |
Host I2C Cable (includes PROJ_ON, HOLD_BOOT, HOST_IRQ signals) |
D | 1 |
LED driver to controller board power cable |
E |
1 |
Controller to DMD board flex cable |
F |
1 |
Red illuminator power cables | G |
2 |
Green illuminator power cables |
H |
2 |
Blue illuminator power cables |
I |
2 |
LED driver to controller board HUD interface flex cable |
J |
1 |
A block diagram for the DLP4620SQ1EVM can be found in Figure 4-10.