Input | ADC Input | Digital Output ADS7042 |
---|---|---|
–10V | –10V |
8000H |
+10V | +10V | 7FFFH |
AVDD | DVDD | Vref | Vcc | Vee |
---|---|---|---|---|
5.0V | 3.0V | 5.0V | +15V | –15V |
Instrumentation amplifiers are optimized for low noise, low offset, low drift, high CMRR and high accuracy. The INA828 instrumentation amplifier preforms a differential to single-ended conversion for a ±10-V range. The INA828 has excellent DC performance (that is, offset, drift), as well as good bandwidth. The ADS8568 is ideally suited to work with the INA828 as the ADC can be configured for a ±10-V single-ended input. To achieve the best settling, limit the sampling rate to 200kSPS or lower. For higher sampling rates see Driving High-Voltage SAR ADC with a Buffered Instrumentation Amplifier. Also, this design example uses unity gain (G=1) to translate a ±10-V differential input signal to a ±10-V single-ended output. For smaller input signals or higher gains, see Circuit for Driving an ADC with an Instrumentation Amplifier in High Gain. This circuit implementation is applicable to Industrial Transportation and Analog Input Modules that require precision signal-processing and data-conversion.
Specification | Goal | Calculated | Simulated |
---|---|---|---|
Transient Settling Error | < 1/2 LSB (±152µV) | NA | –105µV |
Noise | < 20µV | 103µV | 86.6µV |
The following graph shows a linear output response for inputs from differential –14.9V to +14.9V. The input range of the ADC is ±10V, so the amplifiers are linear well beyond the required range. See Determining a SAR ADC’s Linear Range when using Instrumentation Amplifiers for detailed theory on this subject. The full-scale range (FSR) of the ADC falls within the linear range of the instrumentation amplifier.
The bandwidth for this circuit is simulated to be 446.75kHz and the gain is 0dB.
The following simulation shows settling to a 10-V DC input signal with INA828 and ADS8568. This type of simulation shows that the sample and hold kickback circuit is properly selected to within ½ of a LSB (152µV) at 200kSPS sampling rate on ADS8568. See the ADC Front End Component Selection video series for detailed theory on this subject.
This section shows a simplified noise calculation for a rough estimate. The bandwidth estimate was taken from the TINA simulation, and the noise density values are from the INA828 50-μV Offset, 7-nV/√ Hz Noise, Low-Power, Precision Instrumentation Amplifier data sheet. The Kn factor of 1.22 is used because the filter is second order (the INA and output filter both have a pole).
Note that simulated and calculated are close but not exact (simulated = 86.6µV, calculated = 103µV). The difference is because the INA has gain peaking and the filter order is approximated as two but in reality the INA and filter poles are not exactly aligned.
Device | Key Features | Link | Other Possible Devices |
---|---|---|---|
ADS8860 | 16-bit resolution, SPI, 1MSPS sample rate, single-ended input, Vref input range 2.5V to 5.0V | 16-bit, 1-MSPS, 1-channel SAR ADC with single-ended input, SPI and daisy chain | Precision ADCs |
INA826 | Bandwidth 1MHz (G=1), low noise 18nV/√ Hz, low offset ±40µV, low offset drift ±0.4µV/°C, low gain drift 0.1ppm/°C. (Typical values) | Precision, 200-μA Supply Current, 36-V Supply Instrumentation Amplifier | Instrumentation Amplifiers |
Texas Instruments, Source Files for SBAA999, support software