Input Measurement | ADC Input | Digital Output ADS1115 |
---|---|---|
PGA[2:0] = 000, FSR = ±6.144V | 0V to 5V | 0 to 26667 0000h to 682Bh |
VDD | GND | |
---|---|---|
5V | 0V |
Many applications require a large array of measurements using a minimal amount of space. This circuit describes a 16-channel measurement system using four ultra-small ADS1115 devices with an I2C interface. These devices have an accurate internal voltage reference, and can be programmed for multiple input ranges as 15-bit single-ended analog-to-digital converters (ADCs). The ADCs in the system are highly configurable for different data rates and voltage ranges and can even be used for alert functions. Additionally, inputs can be configured in pairs to make an 8-channel measurement system with differential input measurements. The ADS1115 device is available in an ultra-small 1.5mm × 2.0mm X2QFN package that takes up very little space on a board. This circuit can be used in applications such as analog input modules for PLCs, power management on server boards, and a variety of generic measurements.
This circuit uses four ADS1115 ADCs multiplexed to measure sixteen different channels. To do this, the four devices must use different I2C addresses, set by connections to the ADDR pin of each device. The ADDR pin connects to the one of four nodes to respond to a different slave address as shown in the following table.
ADDR Pin Connection | Slave Address | |
---|---|---|
GND | 1001000 | |
VDD | 1001001 | |
SDA | 1001010 | |
SCL | 1001011 |
The ADS1115 device has a multiplexer for measuring multiple channels. In this design, the system cycles through each of the analog inputs of each device. While differential measurements are available, this system is shown by cycling through all of the analog inputs to make single-ended measurements with respect to the GND node.
Devices are configured through the configuration register shown in the following table. Within the configuration register, the MUX[2:0] selects the AINP and AINN nodes for the ADC and sets the input channel for each device. The settings in the table show settings for single-ended measurements. As the ADS111x Ultra-Small, Low-Power, I2C-Compatible, 860-SPS, 16-Bit ADCs With Internal Reference, Oscillator, and Programmable Comparator data sheet shows, differential measurements can be made with settings MUX[2:0] = 000 to 011.
Input Measurement | ADC Input | Device Input Selection |
---|---|---|
Channel 1 | MUX[2:0] = 100 | AINP = AIN0 and AINN = GND |
Channel 2 | MUX[2:0] = 101 | AINP = AIN1 and AINN = GND |
Channel 3 | MUX[2:0] = 110 | AINP = AIN2 and AINN = GND |
Channel 4 | MUX[2:0] = 111 | AINP = AIN3 and AINN = GND |
After cycling through all four channels of the device, the system selects the next device and repeats the cycle.
The ADS1115 ADC has an internal reference for accurate measurements and a scalable gain for the measurement. In this circuit document, measurements shown are all single-ended with the negative analog input attached to ground. Because the ADS1115 device is a 16-bit ADC as a differential measurement, a single-ended measurement has only 15-bits of resolution.
The ADC can be set to one of 6 settings for the FSR (full-scale range). This is the equivalent to having a programmable gain amplifier on the front end of the ADC. The FSR[2:0] bits of the configuration register have settings from ±0.256V up to ±6.144V. When used in a single-ended measurement, the input ranges from 0V to 0.256V up to 0V to the positive FSR value. As mentioned previously, the operating range of the ADC analog inputs is between ground and VDD, even with the FSR set to voltages larger than the VDD. For example, with the FSR set to ±6.144V and VDD set to 5V, the analog inputs are limited to 0 to 5V.
The FSR settings allow for a variety of different measurements from small voltage measurements such as temperature sensors or current shunt resistors, to larger voltage measurements ADC measuring its own supply without the need for a voltage divider.
The settings for the ADS1115 FSR are shown in the following table.
The ADS1115 device can be configured to one of eight data rates, based on the internal oscillator of the device. This data rate has a tolerance of ±10%. The data rate is set by the DR[2:0] bits shown in the following table.
Data Rate Setting | Data Rate |
---|---|
DR[2:0] = 000 | 8SPS |
DR[2:0] = 001 | 16SPS |
DR[2:0] = 010 | 32SPS |
DR[2:0] = 011 | 64SPS |
DR[2:0] = 100 | 128SPS |
DR[2:0] = 101 | 250SPS |
DR[2:0] = 110 | 475SPS |
DR[2:0] = 111 | 860SPS |
The data rate is selected to be 128SPS, which is the default setting of the ADS1115 device. This data rate is the fastest available that gives a noise performance better than one LSB for all FSR settings.
The configuration register sets the mode of operation and configuration of the ADC. Configurations include all of the settings described in the previous sections. Nine fields across 16 bits are used to configure the device. Configuration register field descriptions are shown with bit names and positions, read and write usage, and reset values in the following table.
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
---|---|---|---|---|---|---|---|
OS | MUX[2:0] | PGA[2:0] | MODE | ||||
R/W-1h | R/W-0h | R/W-2h | R/W-1h | ||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DR[2:0] | COMP_MODE | COMP_POL | COMP_LAT | COMP_QUE | |||
R/W-4h | R/W-0h | R/W-0h | R/W-0h | R/W-3h |
OS sets the operational status and starts a single conversion. The MUX[2:0] bits set the input multiplexer to cycle through different measurements. The MODE bit sets the device to single-shot conversion mode. The DR[2:0] bits set the data rate of the device. The remaining fields are used for the ADC comparator settings which are not used in this design. See the ADS111x Ultra-Small, Low-Power, I2C-Compatible, 860-SPS, 16-Bit ADCs With Internal Reference, Oscillator, and Programmable Comparator data sheet for details on the configuration register.
As an example, one ADC is set to measure its own supply to ground, using AIN0 connected to VDD. The FSR is set to ±6.144V, with a data rate of 128SPS. The settings for the configuration register fields are shown in the following table.
Bit | Field | Setting | Description |
---|---|---|---|
15 | OS | 1 | Start conversion |
14:12 | MUX[2:0] | 100 | Single-ended input measurement, AINP-AINN = AIN0-GND, selection of the first channel |
11:9 | PGA[2:0] | 000 | FSR = ±6.144V, sets the ADC to be able to measure the full supply range of 0V to VDD |
9 | MODE | 1 | Operation in single-shot conversion mode |
7:5 | DR[2:0] | 100 | Data rate = 128SPS |
4 | COMP_MODE | 0 | Traditional comparator |
3 | COMP_POL | 0 | Active low |
2 | COMP_LAT | 0 | Non-latching comparator |
1:0 | COMP_QUE[1:0] | 11 | Comparator is disabled |
Combining these bits from the field descriptions, the configuration register values are 1100 0001 1000 0011 or C183h.
To cycle through each channel of the system, start each conversion, wait for the conversion to complete, and then read back the data. Then start the conversion for the next channel. Repeat each measurement for the four single-ended input channels, before moving on to the next ADC. Repeating this sequence for all four ADCs in the system cycles through all channels.
A write to the configuration register starts the conversion and configures the ADC for the proper mode of operation. The communication starts with a write to the I2C slave address of the device. The I2C write is followed by three bytes. The first byte is 01h to indicate the configuration register. The next two bytes are the data written to the configuration register.
A write to device configuration register starts with a write to the selected I2C address (1001000). The next byte is the address pointer which indicates the configuration register of 01h. The write is completed with the two bytes of data to be written to the configuration register. The complete communication of four bytes is shown in the following table.
I2C Address: 1001000 Write |
Address Pointer: Configuration Register |
Configuration MSB: Start Conversion, Set Input, FSR, Single-Shot Mode | Configuration LSB: 128SPS, Comparator Disabled |
---|---|---|---|
1001 0000 | 0000 0001 | 1100 0001 | 1000 0011 |
The master then waits for the conversion to complete. For this example, the ADS1115 device is set to the default data rate of 128SPS. Because the device uses an internal oscillator, there is some variation in the data rate. To verify that the device is read after the ADC completes a conversion, the microcontroller waits for the maximum time required for the conversion to complete. This wait time is the nominal data period plus 10% (to compensate for the internal oscillator variation of the device). An additional 20µs is added for the wake up time of the ADC for each single-shot conversion. The total wait time is calculated in the following equation.
As an example, if the device is run at 128SPS, the nominal data period is 7.82ms. The necessary wait time is:
A read from the device starts with a write to the register pointer for the conversion register (00h) and then another read of two bytes from the same I2C address. The complete communication of five bytes is shown in the following table.
I2C Address: 1001000 Write |
Address Pointer: Configuration Register |
I2C Address: 1001000 Read |
Read Conversion Data MSB | Read Conversion Data LSB |
---|---|---|---|---|
1001 0000 | 0000 0000 | 1001 0001 | xxxx xxxx | xxxx xxxx |
Conversions for the input voltage are based on the full-scale range (FSR) setting of the ADC. The FSR is set by the PGA[2:0] bits in the configuration register.
Even though the ADC is being used for a single-ended measurement, the ADS1115 device is a differential ADC. If the ADC has a negative offset, and the ADC measures a 0V on the input channel, then the ADC reports a negative number. Negative readings are reported in two's complement notation. For example, –1 in decimal is reported as FFFFh in the conversion register.
As previously mentioned, the 16-bit ADS1115 device is replaced by the 12-bit ADS1015 ADC or the TLA2024 ADC. For these devices, the data format is 12 bits with four bits zero padded on the right. A full scale reading is 7FFh and is read from the conversion register as 7FF0h.
The following shows a pseudo-code sequence with the required steps to set up conversions from each channel of the four devices and collect the data after each conversion. It also includes the setup for the microcontroller that interfaces to the ADC.
For each channel, the microcontroller simultaneously sets up the ADC configuration and starts the conversion. The microcontroller waits for conversion to complete, waiting enough time for the conversion and any variation in the internal oscillator frequency. Then the data is read from the conversion register. The cycle continues through each channel of each device. The setup assumes the previous configuration with the data rate set to 128SPS for the wait time for the conversion.
Configure microcontroller for I2C mode
Loop
{
Conversions from four channels of device 1:
{
Write I2C addr 1001000, send 0x01 0xC1 0x83; // start conversion for device 1, AIN0-GND
Wait 8.62ms
Write I2C addr 1001000, send 0x00, read I2C addr 1001000, read two bytes; // Read conversion
Write I2C addr 1001000, send 0x01 0xD1 0x83; // start conversion for device 1, AIN1-GND
Wait 8.62ms
Write I2C addr 1001000, send 0x00, read I2C addr 1001000, read two bytes; // Read conversion
Write I2C addr 1001000, send 0x01 0xE1 0x83; // start conversion for device 1, AIN2-GND
Wait 8.62ms
Write I2C addr 1001000, send 0x00, read I2C addr 1001000, read two bytes; // Read conversion
Write I2C addr 1001000, send 0x01 0xF1 0x83; // start conversion for device 1, AIN3-GND
Wait 8.62ms
Write I2C addr 1001000, send 0x00, read I2C addr 1001000, read two bytes; // Read conversion
}
Conversions from four channels of device 2:
{
Write I2C addr 1001001, send 0x01 0xC1 0x83; // start conversion for device 2, AIN0-GND
Wait 8.62ms
Write I2C addr 1001001, send 0x00, read I2C addr 1001001, read two bytes; // Read conversion
Write I2C addr 1001001, send 0x01 0xD1 0x83; // start conversion for device 2, AIN1-GND
Wait 8.62ms
Write I2C addr 1001001, send 0x00, read I2C addr 1001001, read two bytes; // Read conversion
Write I2C addr 1001001, send 0x01 0xE1 0x83; // start conversion for device 2, AIN2-GND
Wait 8.62ms
Write I2C addr 1001001, send 0x00, read I2C addr 1001001, read two bytes; // Read conversion
Write I2C addr 1001001, send 0x01 0xF1 0x83; // start conversion for device 2, AIN3-GND
Wait 8.62ms
Write I2C addr 1001001, send 0x00, read I2C addr 1001001, read two bytes; // Read conversion
}
Conversions from four channels of device 3:
{
Write I2C addr 1001010, send 0x01 0xC1 0x83; // start conversion for device 3, AIN0-GND
Wait 8.62ms
Write I2C addr 1001010, send 0x00, read I2C addr 1001010, read two bytes; // Read conversion
Write I2C addr 1001010, send 0x01 0xD1 0x83; // start conversion for device 3, AIN1-GND
Wait 8.62ms
Write I2C addr 1001010, send 0x00, read I2C addr 1001010, read two bytes; // Read conversion
Write I2C addr 1001010, send 0x01 0xE1 0x83; // start conversion for device 3, AIN2-GND
Wait 8.62ms
Write I2C addr 1001010, send 0x00, read I2C addr 1001010, read two bytes; // Read conversion
Write I2C addr 1001010, send 0x01 0xF1 0x83; // start conversion for device 3, AIN3-GND
Wait 8.62ms
Write I2C addr 1001010, send 0x00, read I2C addr 1001010, read two bytes; // Read conversion
}
Conversions from four channels of device 4:
{
Write I2C addr 1001011, send 0x01 0xC1 0x83; // start conversion for device 4, AIN0-GND
Wait 8.62ms
Write I2C addr 1001011, send 0x00, read I2C addr 1001011, read two bytes; // Read conversion
Write I2C addr 1001011, send 0x01 0xD1 0x83; // start conversion for device 4, AIN1-GND
Wait 8.62ms
Write I2C addr 1001011, send 0x00, read I2C addr 1001011, read two bytes; // Read conversion
Write I2C addr 1001011, send 0x01 0xE1 0x83; // start conversion for device 4, AIN2-GND
Wait 8.62ms
Write I2C addr 1001011, send 0x00, read I2C addr 1001011, read two bytes; // Read conversion
Write I2C addr 1001011, send 0x01 0xF1 0x83; // start conversion for device 4, AIN3-GND
Wait 8.62ms
Write I2C addr 1001011, send 0x00, read I2C addr 1001011, read two bytes; // Read conversion
}
}
The device starts conversions with a write to the configuration register. This requires a four-byte transaction. Byte 1 is the address write, followed by a byte for the configuration register pointer, and two bytes of configuration data.
When the device reads the conversion, a five-byte transaction is required. Byte 1 is the address write to the device followed by the conversion register pointer in byte 2. Byte 3 is the address read from the conversion register followed by two bytes of ADC data.
Device | Input Channel | Command | Byte 1 | Byte 2 | Byte 3 | Byte 4 | Byte 5 |
---|---|---|---|---|---|---|---|
Device 1 | Channel 1 AIN0 to GND |
Start conversion | 1001 0000 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1100 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– |
Read conversion | 1001 0000 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0001 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 2 AIN1 to GND |
Start conversion | 1001 0000 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1101 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0000 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0001 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 3 AIN2 to GND |
Start conversion | 1001 0000 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1110 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0000 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0001 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 4 AIN3 to GND |
Start conversion | 1001 0000 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1111 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0000 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0001 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Device 2 | Channel 5 AIN0 to GND |
Start conversion | 1001 0010 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1100 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– |
Read conversion | 1001 0010 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0011 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 6 AIN1 to GND |
Start conversion | 1001 0010 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1101 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0010 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0011 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 7 AIN2 to GND |
Start conversion | 1001 0010 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1110 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0010 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0011 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 8 AIN3 to GND |
Start conversion | 1001 0010 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1111 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0010 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0011 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Device 3 | Channel 9 AIN0 to GND |
Start conversion | 1001 0100 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1100 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– |
Read conversion | 1001 0100 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0101 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 10 AIN1 to GND |
Start conversion | 1001 0100 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1101 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0100 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0101 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 11 AIN2 to GND |
Start conversion | 1001 0100 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1110 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0100 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0101 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 12 AIN3 to GND |
Start conversion | 1001 0100 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1111 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0100 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0101 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Device 4 | Channel 13 AIN0 to GND |
Start conversion | 1001 0110 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1100 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– |
Read conversion | 1001 0110 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0111 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 14 AIN1 to GND |
Start conversion | 1001 0110 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1101 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0110 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0111 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 15 AIN2 to GND |
Start conversion | 1001 0110 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1110 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0110 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0111 (I2C address, read) |
<Data MSB> | <Data LSB> | ||
Channel 16 AIN3 to GND |
Start conversion | 1001 0110 (I2C address, write) |
0000 0001 (Pointer to configuration reg.) |
1111 0001 (Configuration reg. MSB) |
1000 0011 (Configuration reg. LSB) |
– | |
Read conversion | 1001 0110 (I2C address, write) |
0000 0000 (Pointer to conversion reg.) |
1001 0111 (I2C address, read) |
<Data MSB> | <Data LSB> |
The following shows an example layout of one of the four ADS1115 devices. RC input filtering is added using 0402 resistors and capacitors. The resulting layout is about 260 mils by 340 mils. This measurement does not include the I2C pullup resistors or the ALERT/RDY pullup resistor. A single set of these resistors are required for each system.
Device | Key Features | Link | Other Possible Devices |
---|---|---|---|
ADS1115 | ADS111x ultra-small, low-power, I2C-compatible, 860-SPS, 16-bit ADCs with internal reference, oscillator, and programmable comparator | 16-bit, 860-SPS, 4-channel, delta-sigma ADC with PGA, oscillator, VREF, comparator and I2C | Precision ADCs |
All trademarks are the property of their respective owners.