Figure 3-1 shows the OPT4001
light sensor design schematic. The light sensor is typically mounted on a dedicated
sensor board and is separate from the main board. The light sensor board is able to
connect to the main board. Refer to the following design tips:
- The SDA and SCL pins require pullup resistors. Customers can add
resistors to the light sensor board or the main board. For the best signal
quality, avoid using long wires or traces. Pullup resistors are not shown in
Figure 3-1 since
these resistors are added to the main board.
- The OPT4001 VDD pin must have a stable, low-noise power supply
with a 100-nF bypass capacitor close to the device and solid grounding.
- The INT test pin is optional. If needed, include a pullup
resistor, since the INT pin is an open drain.
- The PicoStarâ„¢
package does not have ADDR and INT pins.
For all TI light sensors, follow the
PCB layout guidelines in the Layout section of the OPT4001 data
sheet.