SBAA432A april 2020 – july 2023 OPT3001 , OPT3001-Q1 , OPT3004 , OPT3006 , OPT3007
The standalone test platform can evaluate the light sensor without external hardware such as a computer monitor. The display shows the device ID and lux values on the screen of the test platform, as shown in Figure 4-1. The interrupt and address operations are optional. If preferred, the test platform can connect externally to a PC using UART to print the device ID and lux.
TI provides hardware that can simplify the light sensor testing process, such as the microcontroller MSP-EXP432E401Y and sensor plus display board BOOSTXL-EDUMKII shown in Figure 4-2 and Figure 4-3. To use this hardware, place the OPT4001 on the BOOSTXL-EDUMKII board. Plug the BOOSTXL-EDUMKII into MSP-EXP432E401Y and download the correct firmware introduced in Section 4.4. The measured lux is printed on the BOOSTXL-EDUMKII screen and changes with the environmental light conditions. Before testing, confirm that the J5 jumper on the BOOSTXL-EDUMKII connects to the LCD backlight.
If preferred, MSP-EXP432E401Y has a UART to USB interface that can connect to the PC to display the light sensor readings.
The OPT3007 and OPT4001 PicoStar™ tests are similar, but the designer must build conversion boards because the PicoStar package has a bottom-facing sensor.
While any MCU can be used to build the standalone test platform, the BOOSTXL-EDUMKII Educational BoosterPack™ Plug-in Module Mark II user's guide and the SimpleLink™ Ethernet MSP432E401Y Microcontroller LaunchPad™ Development Kit (MSP-EXP432E401Y) user's guide provide all the necessary materials, including the schematic and build of materials.