SBAA445 September 2021 AMC1301-Q1
This section provides a failure mode analysis (FMA) for the pins of the AMC1301-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:
Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.
Class | Failure Effects |
---|---|
A | Potential device damage that affects functionality |
B | No device damage, but loss of functionality |
C | No device damage, but performance degradation |
D | No device damage, no impact to functionality or performance |
Figure 4-1 shows the AMC1301-Q1 pin diagram. For a detailed description of the device pins see the Pin Configuration and Functions section in the AMC1301-Q1 data sheet.
Following are the assumptions of use and the device configuration assumed for the pin FMA in this section:
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VDD1 | 1 | Device high side unpowered. Fail-safe output (see data sheet for more details). | B |
VINP | 2 | VINP stuck low (GND1). Differential output (VOUTP – VOUTN) = –VINN x 8.2 with common-mode voltage approximately 1.44 V. | B |
VINN | 3 | VINN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP x 8.2 with common-mode voltage approximately 1.44 V. | D |
GND1 | 4 | No effect. Normal operation. | D |
GND2 | 5 | No effect. Normal operation. | D |
VOUTN | 6 | VOUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VOUTP | 7 | VOUTP stuck low (GND2). Excess current consumption from VDD2. Device damage plausible if condition is present for extended period of time. | A |
VDD2 | 8 | Device low side unpowered. VOUTP and VOUTN pins are driven to GND2. | B |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VDD1 | 1 | Device high side unpowered. Fail-safe output (see data sheet for more details). | B |
VINP | 2 | Differential output (VOUTP – VOUTN) undetermined, but with tendency to output +FS. | B |
VINN | 3 | Differential output (VOUTP – VOUTN) undetermined. | B |
GND1 | 4 | Device high side unpowered. Fail-safe output (see data sheet for more details). | B |
GND2 | 5 | Device behavior undetermined. VOUTN and VOUTP undetermined. | B |
VOUTN | 6 | Differential output (VOUTP – VOUTN) undetermined. | B |
VOUTP | 7 | Differential output (VOUTP – VOUTN) undetermined. | B |
VDD2 | 8 | Device low side unpowered. VOUTN and VOUTP undetermined. | B |
Pin Name | Pin No. | Shorted to | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|---|
VDD1 | 1 | VINP | VINP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). | B |
VINP | 2 | VINN | Differential input shorted. Differential output (VOUTP – VOUTN) = 0 V | B |
VINN | 3 | GND1 | VINN stuck low (GND1). Differential output (VOUTP – VOUTN) = VINP x 8.2 with common-mode voltage approximately 1.44 V. | D |
GND1 | 4 | GND2 | Not considered. Corner pin. | D |
GND2 | 5 | VOUTN | VOUTN stuck low (GND2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VOUTN | 6 | VOUTP | Differential output (VOUTP – VOUTN) = 0 V with common-mode voltage approximately 1.44 V. Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VOUTP | 7 | VDD2 | VOUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VDD2 | 8 | VDD1 | Not considered. Corner pin. | D |
Pin Name | Pin No. | Description of Potential Failure Effect(s) | Failure Effect Class |
---|---|---|---|
VDD1 | 1 | No effect. Normal operation. | D |
VINP | 2 | VINP stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) = +FS. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). | B |
VINN | 3 | VINN stuck high (VDD1). In case VCM < VCMov, differential output (VOUTP – VOUTN) incorrect. In case VCM ≥ VCMov, fail-safe output (see data sheet for more details). | B |
GND1 | 4 | Device high side unpowered. Fail-safe output (see data sheet for more details). | B |
GND2 | 5 | Device low side unpowered. VOUTP and VOUTN pins are driven to GND2. | B |
VOUTN | 6 | VOUTN stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VOUTP | 7 | VOUTP stuck high (VDD2). Excess current consumption from VDD2 source. Device damage plausible if condition is present for extended period of time. | A |
VDD2 | 8 | No effect. Normal operation. | D |