Entry door – For this test,
the DRV5032 was not able to be influenced by the tamper magnet through
multiple attempts. The LED remained on throughout the testing which shows an
example of the resistance to tampering of the DRV5032.
Sliding glass door – For the
sliding glass door, the magnet was also slowly brought up to the device. The
magnet in this case was also not able to trip the DRV5032 through the
door.