SBAA510 October 2021 DRV5032 , TMAG5170 , TMAG5231 , TMAG5273
Figure 6-1 and Figure 6-2 show the resulting detection field for the Reed switch in the same views done for the DRV5032. Figure 6-1 shows the top-down view, while Figure 6-2 shows the side view. As shown, the Reed switch does have a larger detection distance over the DRV5032, but also has many more detection field variances, which can be unfavorable in security applications where these variances can give way to successful tampering attempts.
Figure 6-3 shows a rotated view to capture detection range on all 3 axes. The detection range is very spontaneous and has no observable symmetrical properties.