SBAA510 October   2021 DRV5032 , TMAG5170 , TMAG5231 , TMAG5273

 

  1.   Trademarks
  2. 1Introduction
  3. 2Reed Switch Overview
  4. 3Hall Effect Sensor Overview
  5. 4Performance Comparison
  6. 5DRV5032 Test Setup and Results
    1. 5.1 DRV5032 Test Setup
    2. 5.2 Understanding the Results
    3. 5.3 DRV5032 Test Results
    4. 5.4 Front Approach Results
    5. 5.5 Side Approach
    6. 5.6 Tamper Susceptibility Testing Setup
    7. 5.7 Tamper Susceptibility Test Results
  7. 6Reed Switch Test Setup and Results
    1. 6.1 Reed Switch Test Setup
    2. 6.2 Reed Switch Test Results
    3. 6.3 Front Approach Results
    4. 6.4 Side Approach Results
    5. 6.5 Tamper Susceptibility Testing Setup
    6. 6.6 Reed Switch Tamper Susceptibility Test Results
  8. 7TMAG5170 Test Setup and Results
    1. 7.1 TMAG5170 Test Setup
    2. 7.2 TMAG5170 Test Results
    3. 7.3 TMAG5170 Tamper Susceptibility Testing Setup
    4. 7.4 TMAG5170 Tamper Susceptibility Test Results
  9. 8Summary

Performance Comparison

This section explains the details of the test setup used for each of the devices as well as the resulting data to provide a suitable comparison of performance and repeatability in detection. For all tests explained in the ensuing sections, the same cylindrical magnet is used leveraging the same approach to the sensor/switch.

Another set of tests for these 3 devices which can be important to product designers is tamper susceptibility. In the case of door and window sensors, it goes without saying that the devices must not be susceptible to tampering through the introduction of an external magnet into the detection field of the sensor. This condition lends itself to a final set of tests to determine how efficient each device is at resisting tampering attempts. The test environment is set up per the following descriptions.