SBAA531 November 2021 ADS8860 , ADS8862 , ADS8881 , ADS9110 , ADS9224R
Table 2-2 lists a short summary of the model pin. For more details on the pins and internal model schematics, see the previous sections of this application report.
Pin Name | Pin Function |
---|---|
INN | Negative analog input pin for the device. |
INP | Positive analog input pin for the device |
Vref | External reference input pin for the device. Connect the external Vref here. |
SampleRate | This pin controls the sampling rate of the ADC. Connect a ±5-V square wave here. Set the frequency of that square wave to the sampling rate at which the device must operate. So, for a 1 Msps device, apply a 1-MHz, ±5-V square wave. |
Vref_ideal | Connect this pin to the ideal value of the voltage reference. If left unconnected it floats to the value of the VREF parameter in the parameter list. So, for example, the ADS8860 has the VREF parameter set to 5 V. If using a nominal 5-V reference, do not connect this pin. This pin calculates the effects of reference droop and reference error in the output signals. |
Vref_err | This is an output pin used to show the reference error. If this output is 0 V there is no error on the output. If the output is 1 mV, the reference has a 1-mV error. |
Vsettling error | This is an output pin used to show the effects of sample and hold settling. This pin compares the steady state ideal input to the ADC to the sample and hold value captured for Vref. If Vsettling_error = 1 mV, than the settling error is 1 mV. Note settling is tested with a DC input signal. This output is not meaningful for AC inputs. |
Vsamp | Shows the output of the sample and hold. |
Tacq | This is an internal signal that shows when the ADC is acquiring (sampling). |
TCONV | This is an internal signal that shows when the ADC is converting (holding). |
ResetSH | This is an internal signal that illustrates when the internal sample and hold is reset. |