SBAA576A may 2023 – june 2023 ADS54J60
The external offset correction feature is an option for system applications that cannot tolerate large variations in the DC, fs/4, and fs/2 interleaving spurs over environmental temperature variations. The internal DC offset can be frozen, read, and loaded externally to calibrate the DC offset over temperature to maintain (but not further improve) the amplitude of the spurs to the levels seen in Figure 3-2 and Figure 3-3.
Section 5 details the required SPI register writes to correctly implement this option. Four configuration files have been created with the writes to further simplify the process.