SBAA578A February   2023  – May 2024 ADS9813 , ADS9815 , ADS9817

 

  1.   1
  2.   2

Introduction

An automated test equipment (ATE) rack contains a variety of electronics subsystems, such as voltage-current (VI) source cards, to enable testing of semiconductors. The function of the VI card is to provide precise and stable voltage and current sources and measurements to test the electrical properties of semiconductor devices. A parametric measurement unit (PMU) generates the stimulus (voltage and current) for the DUT and senses voltage and current. This measurement is available through the multiplexed-voltage-current (MVIx) output of the PMU, where an analog-to-digital converter (ADC) is used to measure the response. The results of these measurements can then be analyzed to determine the electrical performance of the device and to identify any potential defects.

The VI card contains several channels of the subsystem shown in Figure 1. A higher number of VI channels allows parallel testing of DUTs which reduces test-time and cost.

ADS9817 VI Card in an ATEFigure 1 VI Card in an ATE

ADC in Automated Test Equipment Applications

The ADS9813 ADC is an eight-channel, 2MSPS per channel, simultaneous sampling data acquisition (DAQ) system based on an 18-bit successive-approximation register (SAR) architecture. The high channel density of the ADS9813 enables more PMU units to run in parallel, reducing test time and cost. The ability of the ADS9813 to simultaneously sample the input signal on all analog input channels is especially useful in measurements that are sensitive to phase delay between input channels caused by sequential sampling.

The integrated complete analog front-end of the ADS9813 device features an overvoltage input clamp, 1MΩ input impedance, independently programmable gain amplifier (PGA), programmable low-pass filter (LPF), and an ADC input driver. The ADC also has a low-drift precision reference, and an input buffer is integrated for external references. These features reduce the size of the signal chain in the ATE application and the lack of additional external components reduces the error contribution between the PMU output and ADC input.

Design Example

When selecting an ADC for an ATE application, determine the following parameters:

Table 1 Design Target Parameters
ParameterApplication TargetADS9813 ADC

Maximum % Error

(example value from AC/DC voltmeter)

0.005%0.0016%

Settling Time (99.99% of FS)

(example value from LCD panel test)

3.0µs1.73µs
  1. Measurement Accuracy

    The measurement accuracy of the ADC is calculated using total unadjusted error (TUE).

    Equation 1. Total Unadjusted Error (TUE)=Gain Error2+Offset Error2+INL2

    After system level calibration, offset error and gain error can be ignored, and only offset thermal drift and gain thermal drift needs consideration, as shown in Table 2. To reduce thermal drift errors, use a heat sink to reduce the temperature variation of the PMU and ADC.

    Table 2 Measurement Accuracy of ADS9813 Under Various Operating Conditions
    Test ConditionINL (ppm)Offset Error (ppm)Gain Error (ppm)TUE (ppm)Error (%)
    TUE at 25°C15.26495.90183.10528.840.053
    TUE at 25°C after calibration15.260015.260.0015
    TUE at 25°C ±5°C after calibration15.262.5

    3.5

    15.850.0016

    For increased accuracy, the PMU and ADC can share a common reference voltage, as shown in Figure 1. Configuring the reference voltage in such a ratiometric manner cancels the reference drift error.

  2. Fast Channel Selection

    VI cards can have each PMU MVIx output connected to the ADC channel, as shown in Figure 1. Alternatively, the subsystem can use a multiplexer to connect multiple PMU outputs to one ADC channel. Figure 2 shows an example where each PMU has 8 MVIx output channels multiplexed and connected to one ADC input channel. This enables higher channel densities for the VI instrumentation card and reduces cost.

    ADS9817 VI Card with 8:1 PMU:ADC Channel CountFigure 2 VI Card with 8:1 PMU:ADC Channel Count

    The analog input bandwidth of the ADC must be higher when using multiplexers, like in Figure 2, to accurately capture the change in PMU output signals as the multiplexer output is switched. The ADS9813 features two user-selectable analog input bandwidths: Low-noise mode, up to 21kHz, and wide-bandwidth mode, up to 400kHz. The wide-bandwidth mode allows the ADS9813 to sample multiplexed PMU output signals as the device enables step-settling to 99.99% of the full-scale (FS) signal in 1.73µs. The low-noise mode optimizes signal bandwidth versus noise performance in applications which require fewer PMU output measurements, as shown in Table 3.

    Table 3 Bandwidth Mode vs Settling Time and Performance
    Bandwidth ModeSettling Time
    (99.99% of FS)
    SNR (typical)
    Wide-bandwidth (up to 400kHz)1.73µs92dB
    Low noise (up to 21kHz)69.42µs85.5dB
    ADS9817 ADS9813 Settling Response of Low-Noise and Wide-Bandwidth ModesFigure 3 ADS9813 Settling Response of Low-Noise and Wide-Bandwidth Modes
  3. Synchronizing Multiple Devices in a System

    When using multiple ADS9813 devices to sample data at the same instant, the sampling clock can be shared to provide synchronous acquisition of all PMU outputs, as shown in Figure 4. Meanwhile, the data output and data-clock from each individual ADS9813 must be routed together to a dedicated FPGA input to read the data from all devices in parallel.

    ADS9817 Source-Synchronous High-Speed Data Interface With FPGAFigure 4 Source-Synchronous High-Speed Data Interface With FPGA