SBAA615 December   2023 OPT4003-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Light Source Detection
  6. 3Light Source Ratios
  7. 4Design and Calibration Considerations
    1. 4.1 Cover Materials
    2. 4.2 Cover Glass Application Example
  8. 5Near Infrared Components of Common Light Sources
    1. 5.1 Incandescent
    2. 5.2 Halogen
    3. 5.3 Light Emitting Diode
    4. 5.4 Fluorescent
    5. 5.5 Sunlight
  9. 6Summary
  10. 7References

Incandescent

Incandescent bulbs produce illumination by running an electrical current through a tungsten filament. The filament is heated, typically between 2,000 and 3,000 Kelvin, and the inert gas inside the bulb reacts with the tungsten to produce a spectrum that radiates in the visible light region. This visible spectrum is what causes the filament to illuminate, although the peak of the intensity is in the infrared region. The spectral plot of a 2254K incandescent bulb can be seen in Figure 5-1.

GUID-B5810923-D892-4A12-B6DC-9FD56F46AFB5-low.svg Figure 5-1 2254K Incandescent Bulb