SBAS457F October 2010 – September 2019 ADS1118
PRODUCTION DATA.
When the ADS1118 powers up, a reset is performed. As part of the reset process, the ADS1118 sets all of its bits in the Config Register to the respective default settings. By default, the ADS1118 enters a power-down state at start-up. The device interface and digital blocks are active, but no data conversions are performed. The initial power-down state of the ADS1118 is intended to relieve systems with tight power-supply requirements from encountering a surge during power up.