SBAS562B April 2012 – December 2019 AMC1100
PRODUCTION DATA.
Pollution Degree 1—No pollution, or only dry, nonconductive pollution occurs. The pollution has no influence on device performance.
Pollution Degree 2—Normally, only nonconductive pollution occurs. However, a temporary conductivity caused by condensation is to be expected.
Pollution Degree 3—Conductive pollution, or dry nonconductive pollution that becomes conductive because of condensation, occurs. Condensation is to be expected.
Pollution Degree 4—Continuous conductivity occurs as a result of conductive dust, rain, or other wet conditions.