SBAS741B October 2015 – April 2020 ADS1018-Q1
PRODUCTION DATA.
The data in a 32-bit data transmission cycle consist of four bytes: two bytes for the conversion result, and an additional two bytes for the Config register readback. The device always reads the MSB first.
Write the same Config register setting twice during one transmission cycle as shown in Figure 13. If convenient, write the Config register setting once during the first half of the transmission cycle, and then hold the DIN pin either low (as shown in Figure 14) or high during the second half of the cycle. If no update to the Config register is required, hold the DIN pin either low or high during the entire transmission cycle. The Config register setting written in the first two bytes of a 32-bit transmission cycle is read back in the last two bytes of the same cycle.
A continuous SCLK can be used for the entire 32-bit data transfer as long as the SCLK frequency is less than 1 MHz. If an SCLK frequency greater than 1 MHz is used, add a delay between the transmission of the first 16 bits and the second 16 bits to allow for complete decoding of the Config register write prior to the readback of the Config register. Choose the delay such that the time between the SCLK rising edge of the first bit and the SCLK rising edge of the 17th bit is greater than 16 µs.
NOINDENT:
CS can be held low if the ADS1018-Q1 does not share the serial bus with another device. If CS is low, DOUT/DRDY asserts low indicating new data are available.NOINDENT:
CS can be held low if the ADS1018-Q1 does not share the serial bus with another device. If CS is low, DOUT/DRDY asserts low indicating new data are available.