SBAS876C August 2018 – June 2019 ADS9224R , ADS9234R
PRODUCTION DATA.
To enable averaging of two samples, set the EN_DATA_AVG bits in the DATA_AVG_CFG register to 10b. In this mode, the device averages two samples and provides the average of two samples as output data. The output data rate reduces by a factor of two. In this mode, the host must provide two pulses separated by a time of tCYCLE (see tCYCLE for a zone 2 transfer in the Specifications section) on the CONVST pin. The device sets the READY pin high after a time of tDRDY (see tDRDY in the Specifications section) from the second rising edge on the CONVST pin. After the READY pin is set high, the host can read the data by using one of the protocols for reading from the device. The host can read the data while providing the two CONVST pulses for acquiring the next two samples. The host must keep tREAD < [2 × tCYCLE]. Figure 41 provides the timing for the averaging of two samples.