SBAS876C August 2018 – June 2019 ADS9224R , ADS9234R
PRODUCTION DATA.
Dynamic currents are present at the REFP_x and REFM_x pins during the conversion phase, and excellent decoupling is required to achieve optimum performance. Place a 10-µF, X7R-grade, ceramic capacitor with at least a 10-V rating, as illustrated in Figure 84. Select 0603- or 0805-size capacitors to keep equivalent series inductance (ESL) low. Connect the REFM_x pins to the decoupling capacitor before a ground via. Also place decoupling capacitors on the REFOUT and REFby2 pins.