SBAS876C August 2018 – June 2019 ADS9224R , ADS9234R
PRODUCTION DATA.
In clock re-timer protocols, the device sends out data on the SDO lines with synchronized clock on the STROBE line. The data are synchronized to the rising edge of the STROBE pulses. In CRT protocols, the host can use the STROBE output for latching the data. The STROBE for the CRT protocols is either derived from the external SCLK provided by the host or from the internal oscillator. The STROBE signal is held low for protocols other than the CRT protocols.