SBAS894A April 2018 – October 2018 ADS112C04
PRODUCTION DATA.
The device features programmable gains of 1, 2, 4, 8, 16, 32, 64, and 128. Three bits (GAIN[2:0]) in the configuration register are used to configure the gain. Gains are achieved in two stages. The first stage is a low-noise, low-drift, high input impedance, programmable gain amplifier (PGA). The second gain stage is implemented by a switched-capacitor circuit at the input to the ΔΣ modulator. Table 9 shows how each gain is implemented.
GAIN SETTING | PGA GAIN | SWITCHED-CAPACITOR GAIN |
---|---|---|
1 | 1 | 1 |
2 | 1 | 2 |
4 | 1 | 4 |
8 | 2 | 4 |
16 | 4 | 4 |
32 | 8 | 4 |
64 | 16 | 4 |
128 | 32 | 4 |
The PGA consists of two chopper-stabilized amplifiers (A1 and A2) and a resistor feedback network that sets the PGA gain. The input is equipped with an electromagnetic interference (EMI) filter. Figure 43 shows a simplified diagram of the PGA.
VIN denotes the differential input voltage VIN = VAINP – VAINN. Use Equation 4 to calculate the gain of the PGA. Gain is changed inside the device using a variable resistor, RG.
The switched-capacitor gain is changed using variable capacitors at the input to the ΔΣ modulator. Gains 1, 2, and 4 are implemented by using only the switched-capacitor circuit, which allows these gains to be used even when the PGA is bypassed; see the Bypassing the PGA section for more information about bypassing the PGA.
Equation 5 shows that the differential full-scale input voltage range (FSR) of the device is defined by the gain setting and the reference voltage used:
Table 10 shows the corresponding full-scale ranges when using the internal 2.048-V reference.
GAIN SETTING | FSR |
---|---|
1 | ±2.048 V |
2 | ±1.024 V |
4 | ±0.512 V |
8 | ±0.256 V |
16 | ±0.128 V |
32 | ±0.064 V |
64 | ±0.032 V |
128 | ±0.016 V |