SBAS951B August 2019 – April 2020 AMC1336
PRODUCTION DATA.
Figure 48 shows that if a full-scale input signal is applied to the AMC1336 (that is, VIN ≥ VClipping), the device generates a single one or zero every 128 bits at DOUT, depending on the actual polarity of the signal being sensed. This feature can be used for advanced system-level diagnostics to differentiate between system failures caused by missing high-side supply AVDD or input overvoltage events.