SBASA83 April 2021 AMC3336-Q1
PRODUCTION DATA
If a full-scale input signal is applied to the AMC3336-Q1 (that is, |VIN| ≥ VClipping), as shown in Figure 7-5, the device generates a single one or zero every 128 bits at DOUT, depending on the actual polarity of the signal being sensed. In this way, detecting a valid full-scale input signal and differentiating it from a missing high-side supply is possible on the system level.