SBASA84A February 2021 – July 2021 AMC3302-Q1
PRODUCTION DATA
Do not leave the analog inputs INP and INN of the AMC3302-Q1 unconnected (floating) when the device is powered up. If the device inputs are left floating, the input bias current may drive the inputs to a positive value that exceeds the operating common-mode input voltage, leaving the output of the device undetermined.
Connect the negative input (INN) to the high-side ground (HGND), either by a hard short or through a resistive path. A DC current path between INN and HGND is required to define the input common-mode voltage. Do not exceed the input common-mode range specified in the Section 6.3 table. For best accuracy, route the ground connection as a separate trace that connects directly to the shunt resistor rather than shorting AGND to INN directly at the input to the device. See the Section 10 section for more details.
The high-side LDO can source a limited amount of current (IH) to power external circuitry. Take care not to overload the high-side LDO.
The low-side LDO does not output a constant voltage and is not intended for powering any external circuitry. Do not connect any external load to the LDO_OUT pin.