SBASA84A February 2021 – July 2021 AMC3302-Q1
PRODUCTION DATA
Figure 10-1 shows a layout recommendation with the critical placement of the decoupling capacitors (as close as possible to the AMC3302-Q1 supply pins) and placement of the other components required by the device. For best performance, place the shunt resistor close to the INP and INN inputs of the AMC3302-Q1 and keep the layout of both connections symmetrical.
To avoid errors in the measurement caused by the input bias currents of the AMC3302-Q1, connect the high-side ground pin (HGND) to the IIN-side of the shunt resistor. Use a separate trace in the layout to make this connection to maintain equal currents in the IIN and INP traces.