SBASAK4B March 2023 – April 2024 ADS127L21
PRODUCTION DATA
Another method to determine if data are ready is to count clock cycles. This method is only possible when using an external clock because the internal clock oscillator is not observable. After synchronization or conversion start, the number of clock cycles for the first conversion is larger compared to the normal conversion period. The clock cycles of the first conversion is equivalent to the latency time, as listed in the Digital Filter section.