SBASAM0A March 2024 – June 2024 ADS127L18
ADVANCE INFORMATION
The analog inputs of each ADC channel are differential, with the input defined as a difference voltage: VIN = ±(VAINP – VAINN). For best performance, drive the input with a differential signal with the common-mode voltage centered to mid-supply (AVDD1 + AVSS) / 2.
The ADC accepts either unipolar or bipolar input signals by configuring AVDD1 and AVSS accordingly. Figure 7-1 illustrates an example of a differential signal in unipolar supply configuration. Symmetric input voltage headroom is provided when the common-mode voltage is at mid-supply (AVDD1 / 2). For unipolar operation, use AVDD1 = 5V and AVSS = 0V (mid- and low-speed modes offer the option of reduced AVDD1 supply voltage). The VCM pin provides a buffered common-mode voltage to level-shift the signal voltage in the external driver stage.
Figure 7-2 illustrates an example of a differential signal in bipolar supply configuration. The common-mode voltage of the signal is normally = 0V. For bipolar operation, use AVDD1 and AVSS = ±2.5V (mid- and low-speed modes offer the option of reduced AVDD1 – AVSS supply voltage).
In both bipolar and unipolar configurations, the ADC accepts single-ended input signals by tying the AINN input to AVSS, ground, or to mid-supply. However, because AINN is a fixed voltage, the full differential input swing range is lost. Thus, the ADC dynamic range is limited to the voltage swing of the AINP input (±2.5V or 0V to 5V for a 5V supply).
The circuit of Figure 7-3 shows the simplified analog input circuit of each ADC channel. Diodes protect the ADC inputs from electrostatic discharge (ESD) events that occur during the manufacturing process and during printed circuit board (PCB) assembly when manufactured in an ESD-controlled environment. If the inputs are driven below AVSS – 0.3 V, or above AVDD1 + 0.3 V, the protection diodes potentially conduct. If these conditions are possible, use external clamp diodes, series resistors, or both to limit the input current to the specified value.
The input multiplexers of each ADC channel are independently configurable. The multiplexer offers the option of normal or reverse input signal polarities. The multiplexer test modes help verify ADC performance and provide diagnostic tests. The offset test mode verifies noise and offset errors by shorting the internal inputs to the mid-supply voltage. The resulting noise and offset voltage data are evaluated by the user. The full-scale input of each ADC channel is tested for gain error by selecting the –VREF or VREF internal connection. The VREF test signals are at the ADC full-scale signal range. Thus, reduce the value of the digital gain scale registers or program the extended range mode to avoid clipped output codes. The CMRR test mode verifies CMRR performance by applying a dc or ac test signal to the AINP or AINN inputs. The resulting CMRR test data are evaluated by the user.
Table 7-1 shows the switch configurations of the input multiplexer circuit of Figure 7-3.
CHn_MUX[2:0] BITS | SWITCHES | DESCRIPTION |
---|---|---|
000b | S1, S4 | Normal polarity input |
001b | S2, S3 | Reverse polarity input |
010b | S9, S10 | Input short for offset voltage and noise test |
011b | S1, S10 | Input short using a signal applied to AINPn for CMRR test |
100b | S4, S10 | Input short using a signal applied to AINNn for CMRR test |
101b | S6, S7 | –FS dc signal for gain test |
110b | S5, S8 | +FS dc signal for gain test |
111b | S5, S8 | +FS dc signal for gain test |
The input sampling capacitor CIN is part of the simplified input sampling network denoted by the dashed box in Figure 7-3. The instantaneous charge demand of CIN requires the signal to settle within a half cycle at the modulator frequency t = 1 / (2 · fMOD). To satisfy this requirement, the driver bandwidth is typically much larger than the original signal frequency. The bandwidth of the driver is determined as sufficient when the THD and SNR data sheet performance are achieved. Because the modulator sampling rate is eight times slower in low-speed mode compared to high-speed mode, more time is available for driver settling.
The charge required by the input sampling capacitor is modeled as an average input current of the ADC inputs. As shown in Equation 22 and Equation 16, the input current is comprised of differential and absolute components.
where:
where:
For fMOD = 12.8MHz (high-speed mode), CIN = 7.4pF and CCM = 0.3pF. The input current resulting from the differential voltage is 95μA/V and the input current resulting from the absolute voltage is 4.5μA/V. For example, if AINPn = 4.5V and AINNn = 0.5 , then VIN = 4V. The total AINPn input current = (4V · 95μA/V) + (4.5V · 4.5μA/V) = 400μA. The total AINNn current is (–4V · 95μA/V) + (0.5 · 4.5μA/V) = –378μA.
The device incorporates input precharge buffers to significantly reduce the charge required by capacitor CIN. In operation, near the end of the sampling phase, capacitor CIN is nearly fully charged by the precharge buffers. The buffers are disconnected (S11 and S12 of Figure 7-3 in up positions) to allow the external driver to provide the fine charge to the capacitor. When the sample phase is completed, the sampling capacitor is discharged to complete the cycle, at which time the sample process repeats. The operation of the precharge buffers reduces the input current by 99%, and in many cases leads to improved THD and SNR performance. The precharge buffers are enabled by the CHn_BUFP and CHn_BUFN bits of the CHn_CFG1 register. If the AINN input of any channel is tied to ground or to a low-impedance source, disable the AINN buffer to reduce power consumption. A single-ended input application is an example of a low-impedance source.