SBASAR4 October 2024 AMC0311D-Q1
ADVANCE INFORMATION
Do not leave the analog input (INP pin) of the AMC0x11D-Q1 unconnected (floating) when the device is powered up. If the device input is left floating, the output of the device is not valid.
Do not connect protection diodes to the input (INP pin) of the AMC0x11D-Q1. Diode leakage current potentially introduces significant measurement error especially at high temperatures. The input pin is protected against high voltages by the ESD protection circuit and the high impedance of the external restive divider.