SBASAX1 August 2024 AMC0106M25
ADVANCE INFORMATION
As shown in Figure 6-6, the device provides a constant bitstream of logic 0's at the output if the high-side supply is missing. DOUT is permanently low when the high-side supply is missing. A one is not generated every 128 clock pulses, which differentiates this condition from a valid negative full-scale input. This feature helps identify high-side power-supply problems on the board.