SBASAZ0 August 2024 AMC0136
ADVANCE INFORMATION
Place a capacitor at the input of the device (from IN to AGND) to filter the input signal; see the Input Filter Design section. Do not leave the input of the AMC0136 unconnected (floating) when the device is powered up. If the modulator input is left floating, the output bitstream is not valid.