SBASB01 August 2024 AMC3306M05-Q1
PRODUCTION DATA
Do not leave the inputs of the AMC3306M05-Q1 unconnected (floating) when the device is powered up. If left floating, the input bias currents potentially drive the inputs to a positive value that exceeds the operating common-mode input voltage. As a result, the output of the device is undetermined.
Connect the negative input (INN) to the high-side ground (HGND), either by a hard short or through a resistive path. A DC current path between INN and HGND is required to define the input common-mode voltage. Take care not to exceed the input common-mode range as specified in the Recommended Operating Conditions table. For best accuracy, route the ground connection as a separate trace. Connect this trace directly to the shunt resistor rather than shorting AGND to INN directly at the input to the device. See the Layout section for more details.
The high-side LDO is capable of sourcing a limited amount of current (IH) to power external circuitry. Do not to overload the high-side LDO and be aware of derating IH at high temperatures, as explained in the Isolated DC/DC Converter section.
The low-side LDO does not output a constant voltage and is not intended for powering any external circuitry. Do not connect any external load to the LDO_OUT pin.