SBASB12 May 2024 PCM1809
PRODUCTION DATA
The device record channel includes a high dynamic range, built-in digital decimation filter to process the oversampled data from the multibit delta-sigma (ΔΣ) modulator to generate digital data at the same Nyquist sampling rate as the FSYNC rate. The decimation filter can be chosen from two different types only in target mode, depending on the required frequency response, group delay, and phase linearity requirements for the target application. The selection of the decimation filter option can be done by the MD0 pin. Table 6-7 shows the decimation filter mode selection for the record channel.
MD0 | DECIMATION FILTER MODE SELECTION (Supported Only in Target Mode) |
---|---|
LOW | Linear phase filters are used for the decimation in target mode. For controller mode, the device always use linear phase filters for the decimation. |
HIGH | Low latency filters are used for the decimation in target mode. For controller mode, the device always use linear phase filters for the decimation. |