2.2 ADS1x98ECG-FE Operation
To prepare to evaluate the ADS1298 with the ADS1298ECG-FE, complete the following steps:
- Verify the jumpers on the ADS1298ECG-FE are as shown in Figure 2 (note that these settings are the factory-configured settings for the board).
- Verify that the jumpers on the MMB0 motherboard are configured as shown below:
- MMB0 J13A → Open
- MMB0 J13B → Open
- Refer to Section B.2 for details about the MMB0 power supply.
- Install the ADS1298ECG-FE software using the latest software version. The latest software can be downloaded from the ADS1298ECG-FE product page or ADS1198ECG-FE product page. Double click the installer and follow the instruction to complete the software installation. For detailed installation information and screenshots, see Section C.