The ADS8568 is part of a family of related
devices. This EVM hardware and software will support the entire family as all the
devices are pin-for-pin compatable. The ADS8548 is the 14 bit version of the device, and
the ADS8528 is the 12 bit version of the device. The procedure below shows how to modify
the hardware and software to evaluate the other devices in this family.
- Desolder the ADS8568 device an
replace it with the device you want to evaluate.
- Enable the EEPROM for writing. This
is done by changing switch S2 to the top position using tweezers. For details, see
Figure 7-1.
- Connect EVM and start GUI as
described in Section 6.1.
- Use the "Tools" menu to "Load EEPROM"
according to the device that is currently installed. When this procedure is
successfully completed, you will see the status bar at the top of the software
update according to the device installed on the hardware. For details, see Figure 7-2.