Windows™ is a trademark of Microsoft.
All other trademarks are the property of their respective owners.
Table 1-1 lists the related documents that are available for download from Texas Instruments at www.ti.com.
The ADS8860 evaluation module kit includes the following features:
The ADS8860EVM board includes:
The ADS8860EVM is an evaluation module built to the TI Modular EVM system specifications. The EVM by itself has no microprocessor and cannot run software. Thus, the EVM is available as part of the ADS8860EVM-PDK kit that combines the ADS8860EVM as a daughter board with PHI controller using software as a graphical user interface (GUI).