The ADS8688 is part of a family of
related devices. This EVM hardware and software support the entire family because
all the devices are pin-for-pin compatable. Table 7-1 lists other compatible devices in the family. The following procedure shows how
to modify the hardware and software to evaluate the other devices in this
family.
- Desolder the ADS8688 and replace
this device with the device you want to evaluate.
- Enable the EEPROM for writing.
This process is done by changing switch S2 to the top position using
tweezers.Figure 7-3 details this process.
- Connect the EVM and start the GUI
as described in Section 7.1.
- Use the Tools menu to
Load EEPROM according to the device that is currently installed. When
this procedure is successfully completed, you will see the status bar at the top
of the software update according to the device installed on the hardware. For
details, see Figure 7-4.
Table 7-1 Compatible Devices in the
Family
Number of
Channels |
Resolution |
12-Bit |
14-Bit |
16-Bit |
18-Bit |
4 |
ADS8664 |
ADS8674 |
ADS8684 |
ADS8684A |
ADS8694 |
8 |
ADS8668 |
ADS8678 |
ADS8688 |
ADS8688A |
ADS8698 |