SBAU279 October 2020 ADS7038-Q1
The Analog IP can display the FFT of the data captured. This will only display results if the input signal is determined to be an AC signal. Figure 3-14 shows the FFT data analysis display.
The FFT tab displays a table with the fundamental frequency of the input, followed by the noise floor level, SNR, SFDR, THD, and SINAD. The effective number of bits (ENOB) and the number harmonics shown is also displayed in the table.