SBAU294A July 2020 – January 2023 ADC3541 , ADC3542 , ADC3543 , ADC3544
Use the following steps to connect the power supply and mini-USB connections:
Connect 3.3 VDC to TP2 of the FPGA Interposer card. Provide power supply ground to TP1, as required. J10 of the TSW1400EVM can be used to source this +3.3 VDC.
Connect the power cable to the TSW1400EVM at 5-V (minimum 3 A) power supply. Place the power switch (SW7) to the "On" position.
Connect the mini-USB cable to the TSW1400EVM (J2).
Connect the mini-USB cable to the ADC354xEVM (J19).