SBAU359A May 2019 – June 2021
Configure the AC-MB for the USB audio (TDM) and the TLV320ADCx120EVB for the onboard microphone inputs.
The GUI comes with preset files to that can be used for easy initial setup. Select the Load preset option in the top corner of the GUI and load the On Board Microphone setting, as shown in Figure 6-1 and Figure 6-2. Be sure to populate the jumpers described in the settings as described in Table 2-1.
As shown in Figure 6-3, make sure AVDD is selected for the MIC bias voltage and powered up.
The default state for the TLV320ADCx120 is standby mode and, with the exception of the channel digital volume, all device configurations must be done in standby mode. The TLV320ADCx120 does not provide a digital audio output in standby mode. Figure 6-4 shows how to change the mode from standby to active.
When active mode is enabled, any controls not configurable in active mode are grayed out. These controls can be changed again when the device is brought out of active mode. Figure 6-5 shows which controls are disabled.
Audio can now be captured on your PC using the audio program of your choice.