SBAU376A December   2021  – March 2022 TMAG5328

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
    1. 1.1 Features
  5. 2Kit Contents
  6. 3Related Documentation From Texas Instruments
  7. 4Hardware
    1. 4.1 EVM Threshold Adjustment Options
      1. 4.1.1 Adjusting Threshold With DAC
      2. 4.1.2 Adjusting Threshold With Potentiometer
        1. 4.1.2.1 Using the Potentiometer to Estimate the Magnetic Flux Density Sensed by the TMAG5328
      3. 4.1.3 Adjusting Threshold With Fixed Resistor
    2. 4.2 Power Supply Options and Jumper Settings
  8. 5EVM Operation
    1. 5.1 Evaluation With SCB and GUI
      1. 5.1.1 Driver Installation
      2. 5.1.2 Firmware
        1. 5.1.2.1 Updating Firmware on SCB
      3. 5.1.3 GUI Setup and Usage
        1. 5.1.3.1 Initial Setup
        2. 5.1.3.2 GUI Operation
          1. 5.1.3.2.1 GUI Results Page
          2. 5.1.3.2.2 GUI DAC Configuration Page
      4. 5.1.4 Direct EVM Serial Communication
    2. 5.2 Evaluation Without SCB and GUI (EVM Stand-Alone Mode)
    3. 5.3 Head-On Linear Displacement Demo
  9. 6Schematics, PCB Layout, and Bill of Materials
    1. 6.1 Schematics
    2. 6.2 PCB Layout
    3. 6.3 Bill of Materials
  10. 7Revision History

Head-On Linear Displacement Demo

The TMAG5328EVM kit comes with a 3D-printed head-on linear displacement module with an embedded magnet. When connected to the TMAG5328EVM, the module creates a magnetic field that is sensed by the TMAG5328. The module has two portions: a screw and a base. The base is connected to the EVM and the screw is placed inside the base. A magnet is embedded within the screw, which produces the magnetic field sensed by the TMAG5328. Figure 5-22 shows an exploded view of the different components within the module.

GUID-20211108-SS0I-LDTK-F44M-RLSR29HQNNZX-low.png Figure 5-22 Exploded View of the Head-On Linear Displacement Attachment.

When the screw is rotated clockwise inside the base, the magnet gets closer to the TMAG5328, thereby increasing the sensed magnetic flux density. If the screw is turned counterclockwise within the base, the screw increases its distance with respect to the TMAG5328, which decreases the sensed magnetic flux density.

To use this module with the TMAG5328EVM, perform the following steps:

  1. Connect the base of the module to the TMAG5328EVM (see Figure 5-23).
    GUID-20211108-SS0I-RVB0-HKSM-C8H1ZW9NFV13-low.png Figure 5-23 Base Connected to TMAG5328EVM.
  2. Place the screw at the top of the base (see Figure 5-24). As the screw is brought near the top of the base, the sensed magnetic flux density will approach around 2 mT.
    GUID-20211108-SS0I-F12D-DMB1-DZ6Q0MF7PF7G-low.png Figure 5-24 Screw Placed at Top of Base.
  3. When the screw is at the top of the base, turn the screw clockwise to bring screw and its embedded magnet closer to the TMAG5328. After the screw is turned clockwise, the TMAG5328 OUT pin will be asserted low when the sensed magnetic flux density becomes greater than the set BOP. After the screw is fully secured into the base (see Figure 5-25), the sensed magnetic flux density will be larger than the 15-mT BOP maximum that is supported by the TMAG5328, so the TMAG5328 OUT pin will be asserted low and LED D1 will be ON.
    GUID-20211108-SS0I-KDD4-3BTK-BXGQG83PQMT8-low.png Figure 5-25 Screw Fully Fastened Into Base.

For more information on the Head-On Linear Displacement attachment, refer to the Head-on Linear Displacement 3D Attachment user's guide.