SBAU376A December 2021 – March 2022 TMAG5328
The firmware must be flashed onto the SCB to properly communicate to the TMAG5328EVM. After flashing the SCB with the TMAG5328EVM, the firmware does not have to be reflashed on the SCB as long as the firmware is not erased or replaced with the firmware for a different EVM. If the firmware is erased or replaced, the TMAG5328EVM firmware must be flashed onto the SCB again to communicate to the TMAG5328EVM. The latest version of the firmware can be downloaded from: https://www.ti.com/lit/zip/sbac297. It can also be downloaded onto the SCB from the GUI.