- Confirm the power switch on the
TSW14J59EVM is in off position. Connect the power cable to a 12-V DC (minimum
6A) power supply. Make sure the proper supply polarity by confirming the outer
surface of the barrel connector is GND and the inner portion of the connector is
12 V. Connect the power cable to the TSW14J59EVM power connector.
- DAC39RF10EVM can be powered with
12-V DC(minimum 2 A) though the connector jack(J1) on the DAC39RF10EVM or it can
be powered from the TSW14J59EVM via FMC+ connector. There is a switch(SW1) which
can be used to select power from the barrel jack on the DAC EVM or from
TSW14J59EVM through FMC+ connector. Confirm that the power switch for the
DAC39RF10EVM's power supply is set to the opposite position(jack) from which it
should be drawing power. If using barrel jack option connect the power cable to
a 12-V DC (minimum 2 A) power supply. Make sure the proper supply polarity by
confirming that the outer surface of the barrel connector is GND and the inner
portion of the connector is 12 V. Connect the power cable to the EVM power
connector. The Table can used as a reference to power the DAC EVM.
Table 3-1 Powering the
DAC39RF10EVM
DAC39RF10 Powered
from |
DAC39RF10 Power Switch
position |
TSW14J59EVM FMC switch
position |
Power supply
needed |
TSW14J59EVM via FMC+
connector |
FMC(Default
option) |
ON |
12V 6A for
TSW14J59EVM
|
External Supply with
jack on DAC39RF10EVM |
JACK |
OFF |
12V 5A for TSW14J59 and
12V 2A for DAC39RF10EVM |
CAUTION: Make sure the power
connections to the EVMs are the correct polarity. Failure to do so may result in
immediate damage. Leave the power switches in the off position until directed
later.