SBAU395 april   2023 DAC39RF10

 

  1.   Introduction
  2. 1Trademarks
  3. 2Required Equipment
  4. 3Setup Procedure
    1. 3.1  Installing the High Speed Data Converter (HSDC) Pro Software
    2. 3.2  Installing the DAC39RF10EVM Configuration GUI Software
    3. 3.3  Connect the DAC39RF10EVM and TSW14J59EVM
    4. 3.4  Connect the Power Supplies to the Boards (Power Off)
    5. 3.5  Connect the Spectrum Analyzer to the EVM
    6. 3.6  Turn On the TSW14J59EVM Power and Connect to the PC
    7. 3.7  Turn On the DAC39RF10EVM Power Supplies and Connect to the PC
    8. 3.8  Turn On the Signal Generator RF Outputs
    9. 3.9  Launch the DAC39RF10EVM GUI and Program the DAC EVM
    10. 3.10 Programming the NCO
      1. 3.10.1 SPIDAC( NCO only) Operation
    11. 3.11 Launch the HSDCpro Software and Load the FPGA Image to the TSW14J59EVM
  5. 4Device Configuration
    1. 4.1 Supported JESD204C Device Features
    2. 4.2 Tab Organization
    3. 4.3 Register Map and Console Control
  6. 5Troubleshooting the DAC39RF10EVM
  7. 6References
    1. 6.1 Technical Reference Documents
    2. 6.2 TSW14J59EVM Operation
  8. 7Appendix
    1. 7.1 Customizing the EVM for Optional Clocking Support
      1. 7.1.1 LMX->DACCLK | LMX/LMK-> FPGA option (Default)
      2. 7.1.2 EXT->DACCLK | LMX/LMK-> FPGA Clocking Option
      3. 7.1.3 EXT->DACCLK | LMK-> FPGA Clocking Option
    2. 7.2 Signal Routing
    3. 7.3 Analog Outputs
    4. 7.4 Jumpers and LEDs

Launch the HSDCpro Software and Load the FPGA Image to the TSW14J59EVM

  1. Launch the HSDCpro 5.303 or later software.
  2. Click OK to confirm the serial number of the TSW14J59EVM device. If multiple TSWxxxxx boards are connected, select the model and serial number for the one connected to the DAC39RF10EVM.
  3. For Device select DAC from drop down menu.
    Note: If the pop up says No Firmware. Please select a device to load firmware into the board click OK proceed to next step.
    GUID-20230423-SS0I-HDPT-KHPG-N2ZKV1P6DRKC-low.svgFigure 3-7 Launching HSDCpro and Setup
  4. Select the DAC39RF1x_JMODE0 device from the DAC select drop-down in the top left corner.
  5. When prompted, click Yes to update the firmware(wait for Firmware to download).
    Note: If the user configures the EVM with options other than the default register values, different instructions may be required for selecting the device in HSDC Pro. See Section 7 for more details.
    GUID-20230423-SS0I-K7ZV-F8KN-FXTZTBD33SJ8-low.svgFigure 3-8 HSDCpro Setup
  6. Enter the Data Rate as "10.24G" or the desired input data rate. The Data rate value can be referenced from the DAC39RF10EVM GUI. It is displayed on output parameter as shown in Configuration of DAC39RF10EVM GUI.
  7. For DAC Option dropdown select the "Offset Bin" option.( The DAC39RF10EVM gui always defaults to offset binary).
  8. Navigate to lower left side of the HSDCpro GUI to I/Q Multitone Generator section. For # of tones enter 1, for Tone Center enter 1G( 1 GHz or desired frequency), # Samples can be left 65536.
  9. Tone selection should be "Real", since this is JMODE0 , the DUC/ NCO is bypassed. If other JMODE was configured, such that DUC/NCO was used the Tone selection should be "Complex".
  10. Click Create Tones button and then click Send in upper left side of HSDCpro GUI. If a pop appear mentioning the SERDES RATE click OK. The DAC should be sending the programmed frequency to the outputs.
GUID-20230423-SS0I-KQXP-LCN9-XWLBH8C4M79V-low.svgFigure 3-9 HSDCpro Generating the Tone and Sending it to the DAC.
GUID-20230423-SS0I-8HP0-S0NJ-MSMBGN1PSP0H-low.svgFigure 3-10 DAC Output Displayed on Spectrum Analyzer