SBAU402 april   2023

 

  1.   AMC131M03 Evaluation Module
  2.   Trademarks
  3. 1Introduction
    1. 1.1 AMC131M03EVM Kit
    2. 1.2 AMC131M03EVM Board
  4. 2EVM Analog Interface
    1. 2.1 ADC Analog Input Signal Path
    2. 2.2 ADC External Clock (CLKIN) Options
  5. 3Digital Interface
    1. 3.1 SPI Communication
    2. 3.2 Connection to the PHI
    3. 3.3 Digital Header
  6. 4Power Supplies
  7. 5AMC131M03EVM Initial Setup
    1. 5.1 Default Jumper Settings
    2. 5.2 EVM Graphical User Interface (GUI) Software Installation
  8. 6AMC131M03EVM Operation
    1. 6.1 EVM GUI Global Settings for ADC Control
    2. 6.2 Register Map Configuration Tool
    3. 6.3 Time Domain Display Tool
    4. 6.4 Spectral Analysis Tool
    5. 6.5 Histogram Tool
  9. 7AMC131M03EVM Bill of Materials, PCB Layout, and Schematic
    1. 7.1 PCB Layout
    2. 7.2 Schematics
    3. 7.3 Bill of Materials

AMC131M03EVM Operation

The following instructions are a step-by-step guide to connecting the AMC131M03EVM to the computer and evaluating the performance of the AMC131M03:

  1. Connect the AMC131M03EVM to the PHI. Install the two screws as indicated in Figure 6-1.
  2. Use the provided USB cable to connect the PHI to the computer.
    • LED D5 on the PHI lights up, indicating that the PHI is powered up
    • LEDs D1 and D2 on the PHI start blinking to indicate that the PHI is booted up and communicating with the PC; Figure 6-1 shows the resulting LED indicators
    GUID-20230404-SS0I-HQ20-N660-WDXLQXDQBLZL-low.jpgFigure 6-1 AMC131M03EVM Hardware Setup and LED Indicators
  3. Figure 6-2 shows how to launch the AMC131M03EVM GUI software.
    GUID-20230404-SS0I-PCCN-WNW7-VTHHBNK8LLL3-low.svgFigure 6-2 Launch the EVM GUI Software